Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Connectivity in Control Systems Slide 5

One of the advantages of using the TI C2000 device is a digital control system with fast interrupt priorities and fast close control loops. The inputs coming from an ADC, which must be converted into the digital domain, are shown on this slide. There is a transition from the real-time domain into the processor domain, and a feature of the C2000 is low latency between the input and the output.

PTM Veröffentlicht am: