Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
CUS250-Slide3

The CUS250 can operate across an 85VAC to 265VAC input and up to 300VAC for five seconds. The 400Hz operation is possible with reduced power factor correction, but note that like the operation with DC input, this condition has not been tested during safety certification. The unit has active power factor correction to meet the harmonic current specification of EN61000-3-2 and meets class B conducted and radiated EMI.

PTM Veröffentlicht am: