Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
tech 3.3v gen 3
Pericom’s signal switch technology is leading in terms of performance. A key performance parameter is the 3 dB bandwidth; Pericom switches rate at over 8 GHz. Insertion loss for PCIe Gen1, Gen2, and Gen3 applications is very low at -0.58dB, -0.85dB and -1.1dB respectively.
PTM Veröffentlicht am: