Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
LT3088-89-Slide6

As previously stated, the LT3088 is a de-contented version of the LT3089. Because of its current-based reference, the LT3088 only requires a single resistor to set Vout, which is a potential barrier to entry and makes it more difficult for the competition to enter the socket after the PCB board is laid out, compared to the 2-resistor Vout set nature of the other “1117” type competing devices. The LT3088 datasheet contains a section on how to convert from an LT1117 to the LT3088.

PTM Veröffentlicht am: