Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
PWM Modes Image of Infineon's PWM Modes

The 6EDL7141 supports several PWM modes which can be selected to suit the needs of the end product. These include 6-PWM, 3-PWM, 1-PWM, and 1-PWM with Hall sensors. This gives the designer a wide choice of microcontroller size and configuration options to cover a variety of different applications. However, that is not all; the dead time is configurable in 3-PWM as well as both 1-PWM modes.

PTM Veröffentlicht am: