Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Multi-level Class D Amplifier IC Requires NO Inductors

Thanks to the above mentioned nature of multilevel switching topology, users do not need to use big and bulky inductors in the output filtering circuits which are costly and take a large amount of PCB space. Instead, tiny ferrite beads can be used to replace those inductors which saves both PCB space and the BOM cost while allowing the systems to pass EMI tests.

PTM Veröffentlicht am: