Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Introduction to Multi-Level Class-D (cont’d)

In idle conditions when there is no sound being generated, the conventional class D amplifiers are running at 50% duty cycle which is still generating switching losses on the MOSFETs and core losses in the inductor. A multi-level class D amplifier, however, has almost no switching activilities in the power stage and filtering circuits in idle state, hence has tremendously reduced idle power consumptions.

PTM Veröffentlicht am: