Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
10x Better in Idle Power Consumption

Based on the previously explained facts, the idle power consumption of Infineon’s MERUS™ multi-level class D amplifier is only 52 mW at 18 V PVDD, which is only one-tenth that of the conventional class D amplifiers. This greatly helps to improve the system audio playback efficiency performance because idle power consumption dominantly determines the efficiency of an audio system, where the class D amplifiers are mostly running at light load conditions.

PTM Veröffentlicht am: