Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
PTC-Slide12

The SMD PTC chip thermistors are suited as a targeted solution for LED lighting thermal management where the maximum permissible forward current ratings are closely monitored and followed across the full rated temperature range of the LEDs. An SMD PTC offers a low cost solution for the monitoring of an LED array to prevent an overheating condition which would cause the LEDs to fail and overheat in the lighting circuit.

PTM Veröffentlicht am: