Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
PTC-Slide10

In a DC/DC converter application, the SMD PTC can be thermally coupled to offer protection of the power semiconductor whether it is a transistor or thyristor. The circuit example shown here uses the PTC as an effective component for preventing the semiconductor device from overheating.

PTM Veröffentlicht am: