Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
PTC-Slide11

SMD PTC chip thermistors can be used in connection with a standard LED driver IC as a savings performance enhancement to avoid thermal damage of the LEDs at high temperatures in which a shut down of the forward current might be desired. The advantage of his is that it allows for over heating protection for the LEDs with no need for a high end driver IC while allowing the LEDs to operate with a maximum forward current at the standard operating temperatures.

PTM Veröffentlicht am: