Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
ADC-Applications-Slide5

ADI has many ADCs that have the mux on chip. The AD7998 is one example, the 8 channel mux can be sequenced through the different inputs. This has some additional features, like being able to set trigger points for alarms and keeping the highest & lowest reading from each channel.

PTM Veröffentlicht am: