Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
ADC-Applications-Slide17

The AD9246 is a good example of a modern pipelined ADC that is optimized for IF sampling applications with its 650MHz 3dB input bandwidth. It has excellent SNR and SFDR performance at high IF frequencies with very low power. Wireless applications such as wideband base stations where high performance at high IF frequencies is required can take advantage of its high dynamic range; it can support various wireless standards like WCDMA, CDMA2000, TD-SCDMA and WiMax. It can also be used for handheld instrumentation, and test equipment.

PTM Veröffentlicht am: