Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
ADC-Applications-Slide19

A high-speed 4-channel ADC is used when the customer has a diversity receiver. Diversity receivers are used when there are 2 antennas on a cell phone tower that are one-quarter wavelength apart. One antenna will get a stronger signal than the other one. The customer can phase shift the received signals and add them. A quad ADC like the one shown here can accept the demodulated I & Q signals from the 2 antennas.

PTM Veröffentlicht am: