Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Product List
MCW 0406 Slide 3

The “reverse geometry” termination style of the MCW 0406 AT results in optimized heat dissipation from the component to the PCB. Thus, the professional series devices feature high power ratings of 300 mW at an 85°C ambient temperature. The MCW 0406 AT can operate at high film temperatures of 175°C for 1000 hours, compared to traditional resistors typically rated at 70°C with film temperatures of 125°C or 155°C.

PTM Veröffentlicht am: