Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
FPD-Link III Overview Slide 6
Before covering the application challenges, this slide will briefly explain what FPD-Link III exactly is. These products are two pairs of chipsets, the DS90UB901/02 and the DS90UB903/04, that provide sophisticated interface solutions with many technical benefits. These include the high-speed forward channel on serialization and the low speed bidirectional control for inter-integrated circuit (I²C) and GPIO signals. The information is transmitted continuously on just one pair. This replaces the multiple interfaces of wires with just a single pair in the system and allows customers to do more with two. The diagram shows a simple explanation of what is going on. Information is coming at 16 or 21 bits with video data being transmitted in the forward direction. The deserializer then takes the data and sends it to a controller or a display device. At the same time, control data is being sent backward and forward between the serializer and deserializer.
PTM Veröffentlicht am: