Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
FPD-Link III Overview Slide 4
The FPD-Link III solutions are great for automotive applications, specifically multi-camera systems and infotainment displays. The DS90UB901/02 is targeted toward the camera input and driver assist system, as seen on the left. Some of the application challenges in this space are reducing wiring and detecting error. Since cars are becoming equipped with more and more cameras, reduced wiring is needed to keep costs and weight down. These cameras also provide important safety information, so error detection is vital. The DS90UB903/04 is targeted for infotainment displays, either in the center console, navigation system, or rear seat entertainment system. These solutions offer 18 bits of color plus synchronization signals sent from the serializer to the deserializer. One application challenge in this space is dealing with touch screen solutions. The FPD-Link III products provide continual backchannel control, allowing touch screen information to be fed back with very low latency.
PTM Veröffentlicht am: