Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
FPD-Link III Overview Slide 11
This slide illustrates how bidirectional control channel works. The high-speed data is indicated in blue and the low-speed control, backchannel data is shown in orange. What is seen here is that the forward channel driver sends the high-speed data and the forward channel receiver, which is in the deserializer, receives that data at the same time. Then the backchannel driver sends the low-speed data from the deserializer across the same differential pair to the backchannel receiver. The key thing to note here is the continuous transmission of data in both directions over a single pair of wires. That means that both the forward channel driver and receiver are active at the same time that the backchannel driver and receiver are active.
PTM Veröffentlicht am: