Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
open-loop-slide14

Frequency bandwidth or frequency response is another important feature of the open loop hall effect current sensor and is an indication of the ability of the current sensor to accurately measure high frequency input signals with minimal loss in fidelity and attenuation. Small signal currents with frequencies over 50kHz can be measured with less than 3dB of attenuation.

PTM Veröffentlicht am: