Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
open-loop-slide13

Another key feature of the open loop hall effect CS is the ability of the sensor to ‘track’ or ‘follow’ a fast input current waveform. The fastest being a step function with a fast input rise time, or, rate of change of current. The rate of change of current, called di/dt, is the time duration from 10% to 90% of the input signal. Open loop hall effect current sensors are able to ‘respond’ to these high speed signals in less than 5µSec.

PTM Veröffentlicht am: