Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
STM32 Connectivity Line Slide 24

The USB demos running on the evaluation board consist of USB host, OTG demos, and USB Device demos. The OTG demo allows two Evaluation boards to be connected together. The Host demos allow the evaluation board to be connected to a USB device, while the Device demos allow the Board to be connected to a USB host such as a computer. The user interface is managed through the board’s LCD touchscreen. The files can be stored on the USB device or on an SD Card.

PTM Veröffentlicht am: