Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
STM32 Connectivity Line Slide 15

Here is a more detailed example of an audio application. The major features typically required in audio applications are: two audio class I²S interfaces supporting 16 and 32-bit data, a 147.46MHz audio PLL able to provide the master clock with less than 0.5% error, audio sampling frequency ranges from 8 to 96kHz, USB Full Speed OTG with embedded PHY for connecting USB devices such as an MP3 player or mass storage devices, and a SPI peripheral for connecting to SD cards. In this example, the audio files can be stored in either the SD card or the USB devices. The processor is also required to run advanced software such as audio codecs, a file system and the USB host stack for mass storage and audio classes. The STM32’s I/Os are used to connect the buttons, while a second SPI peripheral is used to connect an LCD display. Together, a sophisticated human machine interface can be built for the file browsing and playback functions. To achieve the best audio quality, the STM32’s embedded oscillator accepts audio crystals such as a 14.7456MHz quartz.

PTM Veröffentlicht am: