Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
STM32 Connectivity Line Slide 14

Here are a few application examples requiring USB connectivity. Aftermarket car diagnostic tools, or connecting a computer or USB device to CAN networks requires a USB interface. For home audio devices, a docking station where an MP3 player can be connected to play music on speakers as requires USB. The powerful Cortex-M3 core running at 72 MHz is able to handle a complex user interface in addition to the decoding of music files stored on an SD card or USB mass storage device.

PTM Veröffentlicht am: