Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
ESD Solutions - ESD Suppressors and Multi-Layer Varistors Slide 6
The internal structure of the multi-layer ceramic varistor (MLCV) is basically the same as multi-layer ceramic capacitors (MLCC). It consists of laminates of ceramics and metal electrodes with an external electrode at the both ends. The ceramic materials used in MLCCs are dielectric ceramics whereas the MLCVs use semiconductor ceramics and have basic parameters of varistor voltage and capacitance. The varistor voltage is determined by the thickness of the effective layer while the capacitance is controlled by the effective area (the number laminated layers). Therefore, many different designs are available because of the ease of MLCV construction.
PTM Veröffentlicht am: