Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
ESD Solutions - ESD Suppressors and Multi-Layer Varistors Slide 2

Electrostatic Discharge (ESD) is a major threat to electronic circuitry. ESD can be built-up and delivered to electronics through direct contact with people performing every day activities such as those listed in the table in this slide. The amount electrostatic voltage is dependent on the relative humidity of the air in that larger voltages are built-up when the humidity is low, which is typically during winter months. Integrated Circuits (IC) contained within the electronic circuitry are the most susceptible to being degraded or destroyed. Even internal ESD protection may not be enough, warranting supplemental protection that can be provided by Panasonic’s multi-layer ceramic varistors or ESD suppressors.

PTM Veröffentlicht am: