Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Feat
This slide lists the common features found in all GreenChip SR ICs. The strong drive capability of the driver stage, capable of driving the external MOSFET gate to a voltage of 10 V, ensures that the MOSFET is switched on and off fast, and that the MOSFET is always driven to the lowest possible Rds(on). The fact that the IC discriminates between a primary stroke signal and ringing at low mains ensures that the external MOSFET is always switched on and off at the correct time.
PTM Veröffentlicht am: