Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
GreenChip SR ICs
Modern efficient power supplies are switched mode power supplies rather than a simple linear supply. An often-used topology for building the power supply is the flyback converter. The GreenChip SR is a control circuit which operates at the secondary side of a flyback converter. Depending on the type, it can manage several tasks like driving a synchronous rectification switch, measuring the output voltage and protection against too high output currents. There is a clear trend in the market for higher efficiency year-on-year, enabling power supplies to become smaller and smaller. NXP’s GreenChip SR controllers are a way to increase the efficiency of a discontinuous conduction mode flyback power supply. NXP offers a wide range of controllers, from low-side controllers with integrated feedback control to SR controllers that can also be used high-side. The TEA1791A and TEA1795 are also suitable for resonant power supply topologies.
PTM Veröffentlicht am: