Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
TEA95
Besides the common features of all GreenChip SR ICs mentioned, highlighted on this slide are some additional features of the TEA1795. The TEA1795 features a dual MOSFET control; therefore it can be used not only for dual output flyback topologies, but also for resonant or half bridge topologies. The separate sense inputs ensure independent control of the separate MOSFETs. Using the TEA1795 enables high system efficiency from no-load to full-load.
PTM Veröffentlicht am: