Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
bi normal
However, an audio signal can be either positive or negative. In this case, the protection diode would sometimes be biased in the forward direction during normal operation, making flawless signal transmission on the line impossible. Therefore, bidirectional protection has to be chosen. In addition, for unidirectional and bidirectional protection, the reverse stand-off voltage of the protection diode has to be higher than the maximum allowed voltage of signal; otherwise the diode could break through during normal operation and again make the signal transmission fail.
PTM Veröffentlicht am: