Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
lighting door ex
Electrostatic discharge (ESD) is a phenomena of nature which is best known in the form of a lightning strike in a thunderstorm. Although much less impressive, the zap or ESD strike everyone experiences from time to time when touching a door handle or getting into a car is the very same phenomena. At both events, an electric charge is suddenly transferred from one object or person to another. A sudden electric charge transfer can only occur if the electrical connection has been separated before the event. In a thunderstorm, this happens by the friction between air masses in the storm, but the charge separation can as well be generated by the friction between a carpet and someone's shoes when walking on it.
PTM Veröffentlicht am: