Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
iv before after
This slide shows the current/voltage curves of a varistor and a Nexperia ESD diode before and after one ESD strike. In the left hand graph, the varistor current/voltage graph after an ESD strike, red curve, shows that performance is clearly degraded in comparison to the black curve before the strike. This degradation, after only one ESD strike, in all probability leads to unwanted behavior of the circuit or even to complete failure. On the right hand graph, the Nexperia ESD diode shows no degradation of the current/voltage curve and therefore the functioning of the circuit is not hampered.
PTM Veröffentlicht am: