Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
HumidIcon Digital Humidity-Temperature Sensors Slide 5
The information depicted on this slide is to help better understand what Honeywell’s Total Error Band product specification means. Design engineers want to know the true accuracy of the humidity/temperature sensor that they are using in their product so they do not have to guess or experience a product failure in the field. Honeywell’s Total Error Band specification tells the complete accuracy story, and it is a meaningful and valuable measurement of the sensor’s true accuracy for design engineers. In Honeywell’s product data sheet for the HumidIcon™ sensor, the Total Error Band specification (±5 %RH) and the accuracy specification (±4 %RH) are stated separately to provide a comparison with competitive products that may not list a Total Error Band specification in their product data sheets.
PTM Veröffentlicht am: