Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
dead-time-slide20

If the traces are not tightly couple, not only might they radiate, but the greater inductance will soften the edges of the gate drive currents. Thus, the MOSFETs will not turn on and off as quickly and efficiency will suffer. A highly inductive gate drive trace could also lead to cross conduction of the MOSFETs where the “dead time” is insufficient to ensure both MOSFETs are off at the same time.

PTM Veröffentlicht am: