Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
dead-time-slide12

Shown here is the block diagram of the internal power rails described previously. The DVDD pin is the 1.8V input power to the digital logic. When the Enable pin goes logic level high, the NVM, or non-volatile memory, is loaded in the active RAM. If the enable pin is logic high before the 1.8V input is stable, the start-up logic may not sequence properly and the RAM will not be loaded.

PTM Veröffentlicht am: