Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
dead-time-slide15

The other is the unintended UVLO fault, which needs to delay the enable to ensure the input voltage is ramped up above the UVLO trip point. Usually the UVLO voltage will be set rather high in a case like this, maybe 10V, UVLO for a 12V rail. The Enable Network Equation shown here will help determine the targets needed.

PTM Veröffentlicht am: