Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
AP-Slide7

The AP series follows the traditional C&K nomenclature structure for the Build-A-Switch format. The series designation (AP) is first, followed by the operating force, actuator style, actuator color, illumination, bushing style, termination, contact material and terminal style.  It is important to note that the most up-to-date specifications are in the catalog page available on the C&K web-site at www.ck-components.com. Additionally, it is important to note that there are a number of notes to pay attention to; for instance, illumination is not available with PC terminals.

PTM Veröffentlicht am: