Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
AP-Slide15

In response to customer requests, the actuator caps can be added to the switch after assembly into the control panel. The numerous cap colors and styles allow the flexibility required to solve design challenges. The ability to add caps after the installation of the switch allows the selection of one basic switch, while having the ability to mix and match colors and cap styles. This provides the flexibility to change cap colors and styles as needed in the design. The cap can not be removed from the assembly after being installed and has an orientation feature to prevent spinning or rotating.

PTM Veröffentlicht am: