Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
AP-Slide16

The switching mechanism is a reliable shorting bar for the SPST Normally Open Configuration. The cap can be either installed by the factory or by the user. With or without the actuator cap, the switch is sealed to IP67. There is a rubber dome nested inside the housing and pressed in by the base to provide better sealing. In addition, the rubber dome is protected by the housing.

PTM Veröffentlicht am: