Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
HQ-Slide7

Capacitors can have very low impedances in parallel with a transistor at RF frequencies which can result in several amperes of current flowing through small sections of the circuit at a given time. A small change in the ESR can easily lead to a large power loss in the circuit. The lower ESR and highest Q are a definite advantage in these applications.

PTM Veröffentlicht am: