Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Slide8

These figures show typical waveforms under various conditions. Figure a) shows the low duty cycle that accompanies the large voltage reduction from VIN = 5.5V to VOUT = 0.8V at ILOAD = 600mA. As can be seen in the plot, the minimum on-time achieved is 45ns with a switching frequency of 3MHz. Figure b) shows the load current and inductor current in response to a 300-mA step increase in load current.

PTM Veröffentlicht am: