Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Slide22

In summary, the ADP2102 can be a key component to extending battery life in mobile applications that include a DSP. The ADP2102 can be configured as an external voltage regulator which will reduce the DSP’s core voltage when it does not require the additional power to perform more intensive tasks. Also, for the Blackfin DSP used as the example in this module, using the ADP2102 requires less board space than configuring the Blackfin to use its internal voltage controller. For more information, consult the ADP2102 Data Sheet.

PTM Veröffentlicht am: