Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Slide6

The oscillation described in the previous slide continues indefinitely—at approximately 3 MHz, but deviates as necessary to respond to transient line and load changes—maintaining the output voltage at the programmed value and the average inductor current at the value required by the output load. This approach is relatively new. Previously, the principal approach to DC-to-DC conversion has been a constant-frequency peak-current approach, also known as trailing-edge modulation when implemented in step-down dc-to-dc converters.

PTM Veröffentlicht am: