Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
AS1115-Slide8

For reference the ordering codes of the AS1115 are shown on this page. The table below shows all available ams OSRAM dot matrix LED drivers and compares the most common features. The table shows the maximum LEDs the driver can handle, the average current, and if it integrates a charge pump or has a pin to control an external one. Then it shows the resolution of the PWM, and if the PWM applies to individual LEDs, an LED string, or to the full matrix. The fifth column shows how the analog current can be set. After this there are some features like internal memory, which refers to how many frames or pictures the user can store in the device, if the IC features a reset pin, diagnostic functions, and how many keys can be read back. At the end, the available interface and the package options are shown.

PTM Veröffentlicht am: