Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
ZTP-Slide8

What is a Thermopile? A Thermopile  is a serially-interconnected array of Thermocouples. Each of the thermocouples are formed by the junction of two dissimilar materials. The array is placed across hot and cold regions of the structure with the hot junction thermally isolated from the cold junction. The cold junction would be placed on a silicon substrate for effective heat sinking. The hot junction is formed over a thin diaphragm that thermally isolates the hot and cold junctions. In hot regions, a black body absorbs the infrared energy, raising temperature according to the intensity of incident energy

PTM Veröffentlicht am:
PTM Updated on: 2017-03-27