Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
ZTP-Slide13

The ZTP series of IR thermopile sensors are used for non-contact surface temperature measurement. The ZTP consist of the thermo-elements, flat IR filter, and a thermistor for temperature compensation in a hermetically sealed TO package. There are also a variety of filters available to help maximize performance in specific applications.

PTM Veröffentlicht am:
PTM Updated on: 2017-03-27