Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
ZTP-Slide4

The two formulas, energy and wavelength shown here, show how they are related to temperature. The warmer the source the more energy it emits but as the temperature of the source increases, the wavelength at which most of the energy is radiated at decreases.

PTM Veröffentlicht am:
PTM Updated on: 2017-03-27