Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Select a Tripp Lite Surge Suppressor Slide 6

What causes Line Noise? Line noise has a variety of causes, found inside as well as outside homes and businesses. External Causes - Lightning Strikes: Lightning strikes not only generate damaging surges (voltage increases) but also generate a large quantity of EMI/RFI line noise interference (voltage distortion). Radio & Cell Towers: the air around everyone is filled with a constant stream of radio wave communication, from both radio and cell phone towers. These waves introduce interference into nearby utility power, phone, network and coaxial grids. Internal Causes - Line noise can also be generated within a facility. Lights & Appliances: Fluorescent lights (both the tube and energy-saving, screw-in bulb varieties) generate line noise when it is turned on. Printers and appliances also generate line noise.

PTM Veröffentlicht am: