Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Select a Tripp Lite Surge Suppressor Slide 13

Next, determine how many device cords will need to be connected to each surge suppressor. Tripp Lite offers models with a variety of outlet configurations: 1, 2, 3, 4, 6, 8... all the way up to 24 outlets. Then, determine how far away from the AC wall outlet the surge suppressor will need to be placed. Tripp Lite offers models with a variety of cord lengths: no cord (which plug directly into the wall outlet), 2 ft., 3 ft., 6 ft., 10 ft.... all the way up to a 25 ft. cord.

PTM Veröffentlicht am: