Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
C553x Overview Slide 8

Shown on this slide is the software compatibility and, at a glance, the differences between the four devices. Plus, shown here is how easy it is to move on through the 5504, 5505, 5514, and 5515 devices, which are the higher performing devices, completely software compatible with the C553x family. As can be seen, these processors can run up to 150 MHz and have an external memory interface for parallel memory such as the SRAM, more flash or non-flash.

PTM Veröffentlicht am: