Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
C553x Overview Slide 12

To compliment TI’s low cost devices is the low cost C5535 eZdsp development kit. It includes a small sized development board with a lot of features, such as an on board codec with line in and line out ports, an LCD screen, micro-SD card slot, SPI flash, TI wireless connectors, and expansion connectors for accommodating customers starter boards. It has an on board JTAG emulator, which comes with a free full-featured version of Code Composer Studio 4.0. To help create an out-of-the-box demo for customers TI has also included headphones with a microphone and the micro-SD card with an adaptor. The micro-SD card is preloaded with the USB audio class software and the customer can use the eZdsp board as USB headsets. Just plug in the headphones provided for the complete experience. The LCD screen will show the spectrum analyzer of the music which is being played from the host computer. The complete USB audio class source code is also included on the CD. Texas Instruments is committed to introducing more and more software resources for customers, visit ti.com/C5000 to check for the latest. All of the software that TI is providing will be available to customers free of charge and they can download it from the website or get it with the tool. TI also has a very active and extensive online community and a lot of resources on the E2E community and TI processors Wiki page.

PTM Veröffentlicht am: